Change Product Line
FANUC America Corporation
888-FANUC-US

The Technology Leader in Factory Automation

Discover the possibilities of complete automation

 

 

 

 

 

 

eLearn Based Training Programs (Web courses)

Operations & Programming eLearn Training

Training and Service is only available in the USA, Canada and Mexico

ROBOGUIDE eLearn Training

Mechanical eLearn Training

Specific Features

The eLearn courses are self-paced learning tool that allows users to access information and move through material based on a person’s specific interest or need. The course content and structure is based on an assessment of concepts and skills taught at the FANUC Robotics America’s training facility. FANUC Robotics eLearn courses is, "Training you need, when you need it!"

Features:

  • Easy-to-use interface for simple navigationAccess to specific content through modules that target specific areas of interest or need

  • Provides self-assessment through Progress Check and Mastery Challenge testingAutomatically bookmarks progress through the course based on username logon and password identification, making identification of completed modules easily recognizable
  • On-demand detailed reporting of student’s progress and completion.

Benefits:

  • Self-paced learning when you need it
  • Offers instant feedback, letting students know about areas that may need review
  • Use as a primer to instructor-led courses
  • Diminishes the time users spend away from their primary job function for training
  • Reduces travel expenses to attend basic operations training Can also be used as a refresher course, due to constant personnel changes
  • Provides customers the latest in Instructional Design
 
For more information on this product contact FANUC Robotics at 1-800-iQ-ROBOT or contact us.

To register for an eLearn course: eLearn Registration

.

Robot Operations: This course is available in Spanish too. This is an introductory robotics course that includes basic robot terminology and operational skills. This course covers (the links provide module samples); Module 1) Safety and Cycle Power, Module 2) Moving a Robot in Joint and World Modes, Module 3) Create and Change Teach Pendant Programs, Module 4) Abort, Access, Test and Run Programs
The following link provides a sample of On-Line interactive exercise.  Joint Movement Exercise

Paint Robot Operations: There are 7 modules: 1) Safety, 2 Hardware and Software Overview, 3 Powering on the Robot Controller, 4 Identifying Alarms and Common Fault Recovery, 5 Jogging the robot, 6 Frames, 7 Predefined Positions & Move Menu

HandlingTool Operation & Programming: This course is available in Spanish too. There are seven modules (the links provide module samples); Module 1) Frames, Module 2) Input/Output, Module 3) Program Instruction, Module 4) Modify a Program Module 5) Macro Commands, Module 6) Robot Setup for Production and Module 7) File Management.
This course is a continuation from the Robot Operation eLearn course.

ArcTool Operations & Programming: There are eight modules (the links provide module samples); Module 1) Frames, Module 2) Input/Output, Module 3) Program Instruction, Module 4) Modify a Program Module 5) ArcTool Programming Module 6) Macro Commands, Module 7) Robot Setup for Production and Module 8) File Management. This course is a continuation from the Robot Operation eLearn course.

SpotTool Operations & Programming with Servo Gun: There are 14 modules;
Module 1) SpotTool Intro, Module 2) Servo Gun Master, Module 3) TCP Frame, Module 4) Servo Gun Setup, Module 5) Pressure Calibration, Module 6) Distance, Pressure and Backup Tables, Module 7) User & Jog Frame Module 8) SpotTool Programming, Module 9) Program Instruction, Module 10) Input/Output, Module 11) Modifying a Program, Module 12) Macro Commands, Module 13) Robot Setup for Production, Module 14) File Management.
This course is a continuation from the Robot Operation eLearn course.

iRVision Operations & Programming 2D - There are 8 Modules in the course (the links provide module samples): Module 1) Vision Overview, Hardware and Software; Module 2) Hardware and Software Installation; Module 3) General Vision Concepts; Module 4) Camera Setup and Error Proofing. Module; Module 5) Lighting; Module 6) Tool & User Frame, Calibration Grid Frame; Module 7) Calibration; Module 8) 2D Single & 2D Multiple View Process
This course is a continuation from the HandlingTool Operations & Programming eLearn course.

Force Sensing - There are three modules; Module 1) What Force Sensing is and examples of Force Sensing applications; Module 2) Installing the Force Sensor; Module 3) Programming a Robot which uses Force Sensing.

ROBOGUIDE-HandlingPRO: (View sample of this course) The on-line course provides instructions on how to setup a workcell for our simulation offline programming software.  This course covers;   1) Move a Robot in 3D,  2) Adjust the display,  3) View multiple windows,  4) Edit Robot Properties,  5) Add a Part and define the part in a Cell,  6) Add an End-of-arm Tooling,  7) Defining a relationship between Tool and Part,  8) Create two fixtures for pick and placement,  9) Create/Run a program,   10) Create a AVI file of the workcell, 11) Calibrating the Virtual Workcell to the Real Cell,  12) Add another Robot to the workcell, 13) Set the I/O to avoid robot collision. 

ROBOGUIDE-PaintPRO - (View sample of this course) This eLearn course  provides instructions on how to setup a workcell for our simulation offline programming software.  This course covers;  1) Create a Workcell from the template; 2) Keyboard Navigation; 3) Calibrating the Workcell; 4) Create Paint Paths; 5) Add a New Style; 6) Edit Tracking Boundaries; 7) Add Zones (processes); 8) Add Jobs; 9) Create Repair Panels; and 10) Simulate the Workcell.

ROBOGUIDE-WeldPRO -(View a sample of this course) This eLearn course provides instructions on how to setup a workcell for our simulation offline programming software.  This course covers; 1) Move a Robot in 3D,  2) Adjust the display,  3) View multiple windows,  4) Edit Robot Properties,  5) Add a Part and define the part in a Cell,  6) Add a torch to the robot,  7) Add a dressout to Joint 3, 8) Defining a relationship between Tool and Part, 9) Virtual Teach Pendant, 9) Restart the Controller, 10) Create a welding program, 11) Apply orientation offsets, 12) Adjust the program's default settings, 13) learn all the viewing options after a program run, 14) View the programs profile, 15) Create a user frame, 16) Calibrate the workcell, 17 Importing and Exporting Teach Pendant Programs.

Robot Preventive Maintenance Lubrication - Students successfully completing this course will be able to perform recommended PM Lubrication of all required areas. Grease replenishment, or replacement of Gear-trains and bearings is covered in depth: 1) Safety Intro to Lubrication Functions, 2) Gearbox Oil Level, 3) Bearing Lubrication, 4) Lubrication of Harmonic Drive, Reducers Drive Train & Pivot Mechanisms, 5) General Procedures Position, Vent / Outlet, Grease Input Residual Pressure Release, 6) Custom Gearboxes Grease Change-out Oil Change-out, 7) Bearing Applications

Training and Service is only available in the USA, Canada and Mexico